Best practice in maintenance means the difference between good enough and great. Top quartile performers have lower costs and higher availability using the same resources. This means they can produce more efficiently than they competitors.
2. Best practice in maintenance
means the difference between
good enough and great.
Top quartile performers have lower costs and higher availability using the same re-
sources. This means they can produce more efficiently than their competitors.
3. Advantages of
best practice maintenance
3xMORE LIKELY TO HAVE
LESS THAN 3% OF
REPLACEMENT ASSET
VALUE (RAV)
2xMORE LIKELY TO HAVE
TOP QUARTILE
AVAILABILITY
1.5xMORE LIKELY TO HAVE
MAINTENANCE BUDGET
LESS THAN 3% OF SALES
HIGHER
AVAILABILITY
LOWER
MAINTENANCE
COSTS
LOWER
INVENTORY
COSTS
4. Some characteristics
of top quartile maintenance
MORE LIKELY TO HAVE
TWICE THE PdM
EFFECTIVENESS
5x
MORE LIKELY TO HAVE
LESS THAN 3%
REWORK
4x
MORE LIKELY TO
HAVE >52%
WRENCH TIME
4x
MORE LIKELY TO
INVEST IN MAINTENANCE
TRAINING
7x
MORE LIKELY TO HAVE
CONDUCTED
MAINTENANCE
STRATEGY REVIEW
6x
MORE LIKELY TO
CONDUCT ROOT CAUSE
FAILURE ANALYSIS
4x
MORE LIKELY TO HAVE
OVERTIME LESS
THAN 5%
2.5x
5. How to get there
Avoid Reactive Maintenance
Practice reliability and risk focused proactive maintenance
Implement Best Maintenance Benchmarks
Focus on Continuous improvements
6. Can’t make it alone?
Let SKF get you there.
Learn more at:
http://bit.ly/1RhuPYh